This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR38020: Issue on the open circuit consumption

Part Number: LMR38020

Hi,

I am using this device as a part of a battery project and I have it configured for providing 12 V on the output referring to the "Table 9-1. Typical External Component Values" on the datasheet. Also, I have selected a RT value of 64.9 kOhms which establishes a 400 kHz switching freq following "Table 8-1. Typical Frequency Setting RT Resistance".

The problem comes when I test it's consumption in open loop and, despite the quiescent current is meant to be around 40 uA, I am having up to 20 mA! 

Find attached pictures of my schematic and also of the PCB. May I be missing something in the configuration? I really do not understand why the device is drawing that huge amount of current.

Thank you in advanced,

Nicolas G.