Hi team,
1. If the resister divider or internal FB reference voltage drift and Vout setting unintentionally goes above 9V,
what does occur to the device, system?
In other word, what does limit the maximum output voltage?
2. DC resistance of inductor is recommended to be less than 40mohm in the datasheet.
I would like to use the inductor which is >40mohm.
What does limit the maximum DCR of the inductor?
regards,