This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We are using a BQ27200 Gas Gauge on our product, the .GG file we program is shown below: -
[Device]
Name=bq27000
[Configuration]
Data Units=Engineering
[Gas Gauge EEPROM Constants]
Use CustID3=False
Use CustID2=False
Use CustID1=False
Initial LMD=960
EDVF Threshold=3520
EDV1 Threshold=3672
Initial Standby Load=20.0
Digital Filter Threshold=34.3
Self Discharge Rate (y)=0.20
Taper Current=68.4
Pack Configuration=04
Initial Max Load=205.7
Dsg Rate Comp Gain=5.1
Dsg Rate Comp Thresh=3
Temperature Comp Gain=0.0
Temperature Comp Offset=10
0x76=15
0x77=B8
0x78=CB
0x79=38
0x7A=78
0x7B=86
0x7C=04
0x7D=09
0x7E=37
0x7F=0A
We want to move over to the BQ27210 and would like the profile to remain as close as possible to what we have now.
We only use the following Registers in our system
0x06/0x07 Temp
0x08/0x09 Volt
0x0A Flags
0x0B RSOC
0x0C/0x0D NAC
0x14/0x15 AI
We do not read / use the MLI/MLTTE/SAE/AP registers . I have looked through SLUA429 and see that the bq27x10 is functionally compatible with the bq27x00 if these functions are not needed.
Please could you advise me with the compatible EEPROM values (.GG file) required for the bq27210 based on the above, and also if we need to do anything additional.
Thank you in advance.
Richard