This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM63606: Clarification to have negative output voltage

Genius 14569 points
Part Number: TPSM63606
Other Parts Discussed in Thread: TPSM53604

Hi Experts,

Good day.

If I want to design a positive input to provide negative output (-15V) using TPSM63606, is it possible?

I could see that PGND and AGND from its typical example of datasheet both have different ground reference; are they connected internally? If not, would it be possible to make the Vout as reference side of the overall system and make reading to AGND pins as ouput (-15V)?

Thank you.

Regards,
Archie A.