I designed a circuit for TPS55282 using Webench, 12Vin, 12Vout, Iout=3A. Webench uses a current limit of 15A with a 21kΩ connected to ILIM pin, yet the inductor selected in the BOM saturates at 13A. The inductor is not protected in case of an overcurrent. If I change the design to lower currents, 1A for instance, the different is even greater. Based on the formula in the datasheet, the ILIM resistor should be greater than 27kΩ. Can you please comment on that observation? Should I ignore Webench and use a larger resistor at ILIM?
Thank you!