This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
My customer application condition as below, can you help recommend the inductor spec for below conditions ? thanks!
Vin = 5.5 V ~ 19 V
Vout = 9.2V, 5A
Switching frequency = 400KHz
Hi PY,
Please refer to Chapter 8.2.2.4 in Datasheet for inductor selection, the main specifications that need to be considered are: inductance, saturation current and DCR.
Recommend to choose a inductor with 4.7uH or 6.8uH, Isat>10A.
Regards,
Bryce