Other Parts Discussed in Thread: LMZ30602, TPSM82864A
Hi team,
My customer is looking for a buck module in CT detector to replace EN6310QI.
The requirements are as below:
1. 5V input and 1.1V output.
2. Output current is 0.3A max.
3. Frequency is 2.2MHz and efficiency is 80%
4. QFN or SOP package. (So µSiL (10) of TPSM82821 can't meet it)
Could you please help provide your comments and suggestions?
Thanks a lot!
Thanks & best regards,
Wendy