This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM61495-Q1: need to know Trise, Tfall & VD

Part Number: LM61495-Q1

As part of our design analysis we require following parameters of the Regulator IC LM61495QRPHRQ1

1.  Trise, Tfall - low side MOSFET rise time and fall time

2. Forward direction voltage of low-side MOSFET body diode

Your fast response will help us in great way.

Thanks in anticipation

  • Hi,

    Let me check with the internal team on this.

    Otherwise I can measure the SW node rise and fall time.

    This will estimate the trise and tfall of the low side MOSFET since when high-side is on/ low-side is off and vice versa.

    Will get back to you when I get more information.

    Regards,

    Jimmy

  • Hi,

    In a buck converter, when the high-side turns on, the low-side turns off (vice versa).

    See below for the SW node waveform for a 12Vin|3.3Vout|MODE = FPWM|Rboot = 0Ohm

    In this case the high-side Trise = ~9.5ns and Tfall = ~13.5ns. 

    Control of the Rboot resistor will slow the rising slew rate of the device. 

    The forward bias voltage of the MOSFET should be roughly 0.5V.

    Regards,

    Jimmy