This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM61460-Q1: Ferrite bead instead of Resistor

Part Number: LM61460-Q1

Hi Team,

Our customer is considering to use a ferrite bead in place of the boot resistor for LM61460-Q1. Ferrite bead specifications are 500mΩ DC, 2.2K at 100MHz. Would this work the same, better, or worse when compared to the specified characteristics of the device when 100Ω boot resistor is used?


Kind Regards,

Jejomar