Hello,
On the EVM EN_ICO, FORCE_VINDPM_DET are set to zero.
VAC1=6.5V, VBAT=3.54V , VSYSMIN=2.75V,VBUS=4.29V.
So VBAT>VSYSMIN and VBUS>VBUS_PRESENT.
VBAT_PRESENT_STATUS and VBUS_PRESENT_STATUS are set to 1.
VOC_DELAY=50ms VOC_RATE=30s.
I set EN_MPPT bit , VINDPM=6.3V.
Same test with VAC1=5.0V, VINDPM=6.0V.
It is the same VINDPM minimum value tas without MPPT.
Why this 6.0V minimum value?
Regards,