Hi ~
We ordered 4200pcs TPS70445PWP from TI eStore and it was shipped from TI SPG and USA twice time , But we found some quality issue by our quality department guys.
Firstly, we followed recommended condition of TPS70445PWP to test, and use typical application circuit of Darasheet to do the testing each of 120pcs samples which D/C 2046+5 & 2041+5. Please also check photo of layered fault.
1, 18pcs layered fault while sound scanning. Environment tempature and humidity were normal as 25.6℃ and 53.6%.Fault rate was exceed 15%.
2, 8pcs was found layered fault,which fault rate was exceed 6.7%. same environment as above.
Secondly, all parameters of testing circuit were selected as TI's recommendation, 5v input voltage was in the range of 2.7~6v, output was set fixed out as 3.3v@40mA and 1.2v@40mA with load resistor. then 2pcs aging failure was found after 48 hours aging test when we selected 100pcs testing devices. failure rate is 2%.
3, So we have stopped SMT operatoin already until some new devices was bought from other supplier, Their device testing was NONE of fault .
4, please refer to related layered fault photos and testing circuit as attached documents.
Kindly help refer check it,please.
Best Regards!
Trigger Technology Co.Ltd