Other Parts Discussed in Thread: LM74700-Q1
Dear TI,
We now want to use LM74500-Q1 or LM74700-Q1 for the reverse polarity protection.
The main difference between them is one has the function of reverse current blocking and one doesn't.
We noticed that on the page 13 of the LM74500-Q1 datasheet (<LM74500-Q1 Reverse Polarity Protection Controller>):
(1) LM74500-Q1 is used in the “Load Driving Path”;
(2) LM74700-Q1 is used in the "Logic Path".
We are not clear that the LM74500-Q1 can be also used in the "Logic Path"?
If we choose to use LM74500-Q1, which problems will appear?
Regards,
William