Hi,
I am planning to use LM3671TLX-ADJ and would like to confirm that Ioutmax (per the formula in section 8.2.1.2.1.1 of the data sheet) is referring to the maximum current I need for my application and not the maximum 600mA the part is capable of. Is my understanding correct? I am planning for currents less than100mA. Also since I am going to have current below 100mA are there any other suggestions so that I may maximize efficiency while still keeping my inductor small in size?
Thank you,
HSG