This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2825A-EP: Bus converter questions

Part Number: UC2825A-EP

Hi team,

My customer is considering to use UC2825A-EP for the bus converter application for EOL alternative of UCC28230.

It will be full bridge converter configuration, and Vin = 380V typ, Vout = 270V typ, and Pout=700Wmax.

Could you please help to address the questions below?

- They will use it with open-loop (w/o feedback) and max duty cycle=45%. Is it OK?

- Could you provide the thermal data related to duty cycle if available?

- Could you please provide the application schematic for the full bridge topology?

- Any other recommended full bridge PWM controller which should work under -55C temperature? 

Best regards,

Itoh