This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We’re doing a DPA on the parts listed below. Per MIL-STD-883, TM 2018, SEM is not required for planar die. Is the die fully planar with no oxide steps? Are chemical mechanical polish (CMP) processes used? Or is SEM required?
5962-1222402VHA (TPS7A4501-SP)
5962R9951707VZA (LM117GWRLQMLV)
Thanks,
Hi Michael,
I apologize for the delay. I have reached out to try and find this information for you.
Because of the upcoming holiday the response may be delayed. Please allow 3-4 business days.
Thanks,
Nick
Michael,
Both these devices do not have CMP and no oxide steps in the back end. So, they should be fully planar die.
Thanks,
Prakash L
I just noticed that back in 2018 Alex Segler confirmed for us the 5962R1222403VXC (TPS7A4501RHAKGD) was non-planar and required SEM. Isn't the 5962R1222403VXC similar to the 5962-1222402VHA (TPS7A4501-SP)? Wouldn't they both be planar or non-planar?
Michael,
The back end does not have any oxide or CMP. However, I do see oxide deposition post and pre implant. I am guessing that's considered non-planar based on that, apologize for the confusion. Hope that confirms that both 5962R1222403VXC (TPS7A4501RHAKGD) and 5962-1222402VHA (TPS7A4501-SP) are similar. I did confirm that the other device 5962R9951707VZA (LM117GWRLQMLV) does not have any oxide layers.
Thanks,
Prakash L