Hello, have a question about TPS61322. I need to get 3.6V (100mA max load). I have two solutions:
1) TPS613226A Use 3.3V input voltage (supplying the CPU) formed by LDO connected to Li-ion battery
2) Use a direct connection to the battery and get 5V output with the TPS613222A. And then use LDO at 3.6V
Which of these is the best solution and up to what load current can I use the TPS613226A without an external diode?