This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77216: PINS VERIFICATION AND OUTPUT INFORMATION

Part Number: BQ77216


Hi!
I have some confusion about CELL Reduce in this IC. I want to use 7 cells with this IC. please confirm that attached schematics is good. 

Secondly, I want to use COUT and DOUT for input of my microcontroller (0V LOW, 5V HIGH), can i get these levels at this output or i need some voltage divider circuit in it.

Thanks