This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65150: VGH inrush current

Part Number: TPS65150

Hi Expert,

My customer have an issue of inrush current at VGH ramp up timing.

Vin = 3.3V

Vboot= 10V

VGH =21V~23V

They are using Two-Stage Positive Charge Pump. (from SW node)

At  VGH ramping up, the current of 3.3V rail is around 3Amp_peak. Then, the previous stage power supply is down by current limit.

If they reduce VGH output cap, the input current was down to 1.8Amp_peak.

Do you have any idea for the controlling slew rate of VGH?

And, do you have any other for reducing inrush current? (other than reduce output cap)  

Thanks

Muk