Other Parts Discussed in Thread: TPS92390
Hi Team,
We want to use an LED driver for one of our projects.
We are using white LEDs.
The forward voltage of the LEDs can be anywhere between 3V and 3.5V, so we believe a constant current source will be a good choice.
The supply voltage is 6V.
We want to use both the channels of the IC TPS61150DRCR.
Only one LED is needed on each channel.
1). Is such configuration possible with this IC?.
2). What is the best to choose to drive an LED if its forward voltage is unknown?.