This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7B7702-Q1: SCH

Part Number: TPS7B7702-Q1

Hi Team,

could you kindly check the SCH of 7B7702?

  • Hi Amelie,

    The !ERR pin is open drain so it will currently not operate with a the DNP on the pullup resistor.

    Because you are not utilizing the second channel, it is possible for you to minimize solution size further by removing PR56, but leaving it in does not hurt any operation, the second  and first outputs are isolated from one another so output 1 will not be harmed either way.

    Sense functionality is unused.

    Pin 2 - EN1 is active high, on this schematic only a pulldown resistor to ground is displayed. There is an internal pulldown, so in this configuration, both out1 and out2 are off, and the device will not have any channels in operation. The EN1 signal needs to be pulled high for that

    Regards,

    John