This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62810-Q1: Webench simulation

Part Number: TPS62810-Q1

Hello,

I have a few question about model of TPS62810QWRWYRQ1 in webench. In datasheet of this element is written that if pin COMP/FSET is tied to ground and if at output of device is small capacitance that the switching frequency will be 2.25 MHz (internally set) and that compensation will be as good as possible.

We tried that we 8K06 ohms resistor connected to COMP/FSET and we get 2.23 MHz switching frequency and good compensation but we would like to remove this resistor and when we tried to connect this pin to ground (via 0 ohms resistor) we get that the switching frequency is infinityHz.

Is there a problem with model of device and can we do this? Will compensation be better with resistor connected to this pin?

Also, can we expect and when a Start-up simulation option for this model? 

Thanks in advance and looking forward to your reply!

Best regards,

   Miloš