I have been running simulations in PSPICE for the LMZ34002. When I modified the steady state design to incorporate a load step, I am seeing that the when the step occurs, an overshoot happens and then settles back to -15V. When the step goes away, you'll see the undershoot, but it never recovers like how the overshoot recovers unless it needs much more time than I set at 1ms for the load step pulse.
I took a look at the webench design and it seems much more reasonable.
Input: 25.2V-30.8V
Output: -15V
Iout: 0.3A
Below are screenshots of my simulation design and waveform. I'm using a switched resistor load. It initially has a 10k load for 1.5mA, and then a switched Rload of 50ohms for 0.3A. Any ideas? I'm looking to get better regulation around +/-250mV for a 0.3A, looks like the only way to achieve that would be more bulk capacitance? Would you agree?