Other Parts Discussed in Thread: TLV840, BQ25616, , TPS61230A, BQ25611D
Hi team,
The customer would like to find a kind of chip which can meet the following requirements:
1. About 2 A charging, 2 A discharging
2. output 5 V (output voltage should be higher 5.5 V, or it's adjustable)
3. Automatically detect load discharge, do not switch on or off
4. 2-4 indicators - includes low-battery, status, full-charge, and can be used for portable power supplies
5. 4.2-V single-cell Li-ion battery charging
Could you help give some advice? Thanks.
Best Regards,
Cherry