Hi Team,
In the data sheet of the LM4041-N there is probably an error. The maximum current is given at various points with 12 mA.
But section says 6.3 "1200µA recommended operating Conditions" what would be 1.2mA. Should 12.000µA stand here?
I saw in the competitors data sheet that they note the reverse current value as 12mA for the adjustable part.
Thanks
Jan