This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS737-Q1: When can tps737-q1 output 1A?

Part Number: TPS737-Q1

Hi Expert,

As you know, TPS737-q1 can output 1A. But the use case  could be very limited. As an example, I want 5Vto3.3V @1A. The power dissipated on TPS737-q1 is about 1.7W. The junction  temp could be 88℃. If we think ambient temp is 85℃, it exceeds the range. I just don't know exactly under what situation it can be used since I think 1.7V voltage drop is small enough. Thanks!

BR, 

Elec Cheng