This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS56637: Temperature cycle test

Part Number: TPS56637

Hello team,

Do you have data of temperature cycle test with TPS56637?

Condition what customer is interested in is below.

  • VIN=24V, VOUT=5V, IOUT=3.28A
  • Ta cycle between 0C and 70C(10 times cycle with 30min for each temperature condition)

My customer would like to confirm if TI has some data to say that TPS56637 would not get damaged with above condition or more severe condition.

Do you have such reference data for the temperature cycle test?

Best regards,