I am working on BMS application using BQ79656 ICs. I want to connect multiple BQ79656 Ics through Ring architecture.
As per datasheet, for ring architecture Base BQ79656 Ic will be interfaced with BQ79600 Ic. Low channel of ISO SPI of BQ79600 Ic will be connected to high channel of ISO SPI of highest number of BQ79656 IC. Please see below image. But BQ79600 IC is not available any where. Can you suggest some alternative ICs ?
Also can we connect low ISO channel of base BQ79656 with high ISO channel of highest number of BQ7956 IC to complete ring architecture. Base BQ79656 IC will interface with MCU through Isolated UART. Is it possible ? I attached block diagram of this architecture.