Other Parts Discussed in Thread: TPS54335A
Hello,
I am considering the circuit below.
The PGOOD signal of TPS65261-1 controls two TPS54335A.
EN of TPS54335A is set to turn on when VIN is 9V.
The reason is to start TPS54335A after TPS65261-1 is completely started.
It is assumed that the TOP resistance R11 of EN is 100 kΩ and the BOTTOM resistance R12 is about 15 kΩ.
Does the circuit I thought of work normally?
If you have any problems, please give me your opinion.
Best regards,