This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22810: Inquiry about the application design

Part Number: TPS22810
Other Parts Discussed in Thread: TPS22918

Hello,

My customer is designing a power block using the TPS22810 and TPS22918.

According to the datasheet, the application circuit contains CL and RL components as shown below.

What are the roles of the CL and RL components?

Are The CL and RL components mandataoy ? is it okey to remove these parts from the customer's board?

Thank you.

JH

  • Hello JH,

    RL and CL represent the customer's potential load. They are not required; however, there is a recommended Cout (output capacitor as close to Vout pin as possible) of 0.1uF. 

    Regards,

    Kalin Burnside