This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
I am testing thermal capability on EVM Iout=13A,vout=5V 600KHz, room temperature=22.3°C
I know “TJ = TA + (Thermal resistance × Power)”, and I used webench to get the power loss (2.257 W) and Tj. However the calculated and simulated Tj is only around 70°C
which is much lower than the top temperature (108 °C) I sensed with IR imager and it doesn't make sense.
1.Why would estimate Junction temperature is lower than top temp I measured, did I miss something? should I see ambient temperature as room temperature?
2.Why the junction to ambient thermal resistance is different between JEDEC and EVM?
Regards,
Fred
Hi Fred,
Our US team will reply you tomorrow.
Hello Fred,
I've also attached two Application Reports in which I believe will be helpful in regards to thermal measurements.
Regards,
Alejandro
Hi team,
Thanks
1. my point is, I can use top case temperature and ΨJT to get junction temperature as well, and it will be like 110C, which is way more larger than the Tj (70C) I calculated with Ta and RθJA .
and I know the fact is junction temperature will always be higher than top case temp (108C). However Wenbench show the Tj is only close to the 70C, so I'm confused.
Which one should I believe? 110C or 70C
2. Does below description means ambient temp has its own definition, we can't just use room temperature?
Regards,
Fred
Hi Fred
Just to be sure - can you please confirm that the load current of 13A is accurate? Also, can we rule out any calibration issues with the thermal camera?
Regards,
Gerold
Yes, I confirm I use 13A and it's accurate, and I don't think IR imager could have any problem that will affect so much (70C to 110C)?
is webench Tj analysis accurate? what's equation is it base on?
Hi Fred,
The WEBENCH analysis is more accurate. For example, see Thermal Performance of EVM on datasheet Section 10.2.1. The EVM at 20A measures only 88°C.
Regards,
Alejandro
Hi team,
Thanks for the feedback, actually this is an qualification for HPE, so might be extra support
1.So you mean my measurement is not accurate, any Idea why my IR imager sense overhigh temperature?
2. What does "2.54cm to the horizontal means"? does this mean it's not recommended to use room temperature?
Hi Fred,
Regards,
Alejandro