When VBAT < 1.5, and I out < 50 mA. it looses regulation, what could be the reason?
I am using electronics load.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When VBAT < 1.5, and I out < 50 mA. it looses regulation, what could be the reason?
I am using electronics load.
Hi Sir,
TPS613221A should work properly even Vin is below 1.5V. Would you mind test the voltage on C2 pin and also VOUT when it is out of regulation? Do you have any waveform on inductor current, output voltage and SW voltage when it is out of regulation? Please also share layout to me. Thanks!
-Wenhao
Hi Ayman,
The ringing is normal when converter enters DCM operation. I add your friendship. You can share the AD file to me. Please kindly check voltage on C2 and also VOUT voltage when you see it is out of regulation.
-Wenhao