Hello,
datasheet says that active EMI is automatically enabled at 40% of the current limit. However, we are unsure how will conducted emissions look like in our application, at which level they will become over the line, therefore we would like to have it controlled from microcontroller or enabled by default. And here comes the trouble:
This pin is as well used for configuring Spread spectrum, primary/secondary etc. at the startup during the first 50us. Could you propose or share general do's and don't do's?
-When this DCDC is powering up, the rest of the board is still unpowered. I assume that potential CPU control circuit must be tri-stated during the LM25149 start-up in order not to confuse the "power-up configuration" control logic?
-What is the maximum voltage level, is it ok to use VCC as a high voltage level?
-Any safe simple trick that can be used to enable AEF by default, without affecting the power-up configuration? (if we want to skip the MCU control)
Thank you for any tips
Petr