Other Parts Discussed in Thread: TPS53353, TPS53355
Hello team,
I would like to confirm if TPS53353DQPR or TPS53355DQPR could be considered as an alternative for TPS53318DQPR.
From the datasheet, TPS53353 and TPS53355 seems to be pin compatible with TPS53318, while continuous output current and 5 pin termination seems to be different.
Could you check these questions below?;
- Q1) 5 pin is N/C for TPS53353/TPS53355, and ROVP for TPS53318. Is it possible to replace TPS53318 with TPS53353/TPS53355 by simply removing the resistor or capacitor connected to the ROVP pin's circuit?
- Q2) The continuous output current is 20/30A for TPS53353/TPS53355, and 8A for TPS53318. Is it possible to limit the output to a maximum of 8A by changing the resistance value of the TRIP pin?
We would also like to know it if there are any other concerns regarding replacement.
Best Regards,
Ryotaro Fukui