Other Parts Discussed in Thread: BQ78350, BQ76940
Hi Sir,
BQ78350 datasheet shows , VCC relative to VSS maximum ratings is 2.75V
I connect BQ78350 VCC by BQ76940 regout (3.3V),
does this regout 3.3V will damage the BQ78350 ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
BQ78350 datasheet shows , VCC relative to VSS maximum ratings is 2.75V
I connect BQ78350 VCC by BQ76940 regout (3.3V),
does this regout 3.3V will damage the BQ78350 ?
Hello User,
You are correct, the 3.3-V REGOUT would damage the BQ78350.
You would need the BQ76940 device with a REGOUT that outputs 2.5-V if you want to use it to power the BQ78350.
Best Regards,
Luis Hernandez Salomon