Hello,
I am designing a board based on the TPS61288 boost converter.
In my application I have a VIN (6V to 8.4V, 2S Li-ion battery), VOUT 13V and IOUT max 3.5A.
I calculated the values of the following components, making calculations based on the formulas in the datasheet:
R1 = 274 kΩ
R2 = 13.3 kΩ
L = 2.2 µH
Coutput = 114 µF (22+22+22+47+1)
Cinput = 69 µF (22+47)
I am trying to calculate the value of the components Rc, Cc, Cp for the phase compensation, using the equations 12, 13, 14 of the datasheet, but I can not do because I don't have the values of Ro and RESR, and it is hard to find the real values of Couput, Cinput under the various conditions(derating).
So, is the compensation network very sensitive or can I use the same network of evaluation board even if the boundary conditions are different?
I look forward to receiving your feedback.
Thank you!