This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM63606: Output 2.5V

Part Number: TPSM63606

Hello,

I want to set the output to 2.5V. with nominal input 28V

 

1- Frequency Fsw:

On the datasheet table 8-1 (p16), the suggested Fsw is between 650 to 900kHz.

But with the equation 6 (p18) -> Fsw = 570kHz.

and with the eval board TPSM63606EVM datasheet : for 2.5V, Fsw is set to 500kHz

and with Power designer, the frequency is set to 730kHz

Maybe i miss an information, but is it better to stay in the suggested Fsw or to set like the eval board ?

It's just to choose the correct Rt value for this Vout.

 

best regards