Other Parts Discussed in Thread: TPS51916
Webench support team,
I can't get a simulation result due to the specification limitation of the external FET used in Webench-Power-Designer. The below is an error message.
How can I change the FET configuration from a single FET to Dual FET in parallel?
My simulation device is TPS51916. The simulation condition is follows.
- Input Voltage = 9V - 18V
- Output Voltage = 1.1V
- Output Current = 20A
- Ta=30degC