When the BQ4050 deadband current is set to 3mA and the battery voltage drops to EDV0 3V after a period , the RSOC is still 96%.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When the BQ4050 deadband current is set to 3mA and the battery voltage drops to EDV0 3V after a period , the RSOC is still 96%.
Hi Shirish,
Yes, the voltage drops below 3V after storage several months by battery consumes power. The battery consumes current is less than 1mA.
If this is caused by self discharge or similar reason, then you can set the following data memory configuration to let the gauge know to compensate for it.