Hello,
I have problem with predischarge.
I set these regiesters:
FET OPTIONS 0x1D
PREDISCHARGE TIMEOUT 30
PREDISCHARGE STOP DELTA 0
I have programmed two seconds period toggle of output. I have capacitor 470uF with electronic load set to 2A.
I made SW preconfiguration and I'm switching ON and OFF output by command FET_ENABLE. Behaviour of BQ is very strange.
If load is OFF then sometimes it makes predischarge phase, sometimes not, (mostly not).
If load is ON then predischarge never happened.
First picture is schematic of predischarge.
Second picture is working predischarge no load,
Third picture no predischarge with load,
Fourth picture no predischarge with smaller load (blue curve is current probe)