This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65185: Power Up Troubleshooting

Part Number: TPS65185

Hi,

I'm using a TPS65185 chip to power up a E-ink screen (ED060) and I am having some issue powering up the EPDC. The device is set to ACTIVE through I2C communication.

With the screen unplugged, the power rails are in regulation.

(VN in Yellow - VNeg in Blue)

Otherwise, once the display is plugged into the connector, the PMIC doesn't power up and the interrupt register shows a VNeg under voltage error, and the Power Good register shows 0xA0 (when 0xFA without the display).

(VN in Yellow - VNeg in Blue)

I tried to increase the delay between the ramp up of the rail, without success. The only load on the rail is the EPDC (so I don't think the current exceed the capacity).

I tried different displays, and I experienced the same issue. Any idea of what could cause this problem?

Best,

Vincent