This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25118: Generate 4 isolated output

Part Number: LM25118

Dear teams,

Whether LM25118 can implement following requirements?

Vin: 5-36V

Vout: 4 output with voltage 8V; Output current are 30/30/30/80mA, totally 170mA.

Customer is planning to achieve isolation at the output side with ratio 1:1 transformer to do that.

If you think LM25118 is not appropriate, could you help recommend one device?

Thanks!

Dylan