Hi Team,
A customer found a discrepancy with the datasheet for TPS7A84A.
The customer pointed out that Figure 6-8 shows 60dB PSRR for 10Hz to 10MHz bandwidth, at Vin = 1.3V, Vout = 1V, Iout = 3A
However, these results appear to contradict Figure 6-5.
what should the customer do for only adding Cout 47uF,10uF,10uF with VBIAS?
Figure 6-5 and 6-8 have almost same test conditions but have very different PSRR result
Which is correct?
Hoping you can help.
Regards,
Marvin