This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77908A: Cell balancing for LiFePo4 (4s)

Part Number: BQ77908A
Other Parts Discussed in Thread: BQ34Z100-G1, BQ40Z50-R2, EV2400, BQ40Z50, BQ4050

Hello there,

We are currently looking for an autonomous (or semi-autonomous) cell balancing IC that could be used with a 4s LiFePo4 chemistry cells. We have decided to use the bq34z100-g1 for gauging and considering the bq77908A for balancing and protection. Issue is that it seems that this IC is intended for Li-Ion and Li-Polymer packs.

Question is- can the IC be used with LiFePo4 after the registers are adjusted?

If there is a better fit for this in the TI portfolio, I would appreciate the suggestion. We are considering using an MCU that would be a data collection node for the bq34z100-g1 and the cell balancing IC, before the end data is exposed to the end system (for instance the if the balancing algorithm would not be fully automated). If possible however, it would be best to not use any additional MCU's...

I would appreciate all feedback and suggestions.