Hello,



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Hello Roger,
Have you seen these two threads?
It looks like this is a duplicate thread. SOH is not meant to change very suddenly like this, but pulsed loads at cold temperatures are the most difficult for gauging. Also, have you see Wyatt's suggestion on the second thread? See if you can implement the experiment he suggested in the second thread by changing deltaV to be negative. Also, I believe you should be able to post on the other thread, even if you did not start it. Lets try to keep everything to one thread so it doesn't get confusing.
thanks,
Alex M.