I am designing with the LM2623A controller.
Vin min = 1.8V
Vin max = 4.5V
Vout = 9.5V
Iout = 0.2 A
In the datasheet, it says selecting C3 is a "trial and error" process. But I was hoping to get some guidance as to what value I should even start with. Example circuit in the datasheet has 4.7pF.
Following this TI doc
https://www.ti.com/lit/an/snva731/snva731.pdf?ts=1644852689362
It says that the duty cycle is:
D = 1 - ((Vin * eff)/Vout)
In my case D would be 85% with an 80% assumed efficiency. The part does imply a max duty of 90%. So I would be cutting it close.
And because my input voltage changes as the battery discharges, I will need a series resistor to C3, according to this doce
www.ti.com/.../snva050d.pdf
Questions:
1. Does this part have a spice model (TINA, LTSpice) in which I could use to help select C3? Or is that not an accurate option either?
2. What value of C3 should I start with in my case? And what resistor in series should I use?
Any help, tips or tricks are appreciated.