Hello,
I am working with "TPS65265RHBR triple channel DC to DC regulator.
the circuit is configured with a particular power sequence as "BUCK1-<BUCK3->BUCK2".
Configured Enables pins as mentioned in the datasheet.
but the sequence is not as per"BUCK1-<BUCK3->BUCK2".
I am getting a power sequence as "BUCK1-<BUCK2->BUCK3".
Between BUcK 1 to BUck 2, I can observe a delay of around (0.2ms -0.3ms), and between Buck 2 to Buck 3, I can observe a delay of (2ms to 2.5ms).
So can someone review my schematic and let me know why do I get such an issue.,
-
NOTE:
Also, I try the below possibility tests too.,
1. I tried connecting the MODE pin to VCC (3.3V) and also by floating the MODE pin but there is no change in a power sequence.
2. Also I tried by connecting PSM pin VCC (3.3v) and also by floating the same pin but there is no change in a power sequence.
3. I tried different delays to EN3 pin as 2ms,10ms,12ms but there is no change in a power sequence.
4. I try to connect the MODE pin to High (TPS65265 IC 1st pin),in the TPS65265 1st pin we get 6V. [This one i tried because in EVK it was mentioned to give to 1st pin of TPS65265 IC for high].but there is no change in a power sequence.
5.