Dear Sir,
We are using TPS65100 for Powering LCD where we need AVDD=10.4V, 400mA, VGH = 16V, 4mA, VGL = -7V, 4mA, and VCOM = 3.6V. We are facing some problems with the below-attached schematic, Some time start and build all power supplies as normally required on Power up, but sometimes do not start and build up any required power rail.
Please suggest any corrections to be made to solve the above issue.