Hi, TI support team
Inquire to the customer to recommend the TPS61236P product as an alternative to the products below.
- MP3423 / MAXIM
1. It enters into PFM mode during light load. What is the light load level? (how many mA?)
2. If measured in actual EVM, is it possible to measure at the level of item 1?
3. The datasheet describes the operation according to the high/low of the EN pin.
3-1. If the EN pin is low when Vin is input, is Vout at 0V level?
3-2. Is it true that EN is always true disconnection when low?
Please give me a quick reply.
Thanks.
Regards,
MJ