Other Parts Discussed in Thread: UCD90160, UCD90120, UCD90320
The UCD90320U has additional protection from Single Event Upsets compared to the UCD90320, the UCD90120 and the UCD90160, it has the ULA molding and the SEU detection algorithm (8.4.20 Single Event Upset). My questions are:
- The ULA molding is not available on the UCD90120, or UCD90160 are there plans to add it.
- Was the ULA molding and SEU detection added for a particular reason, were the other parts found to be susceptible to SEU events.
- For the non ULA molded, non SEU detecting devices, Did their internal fault management/watchdog timer reset the device in the event of a SEU event.
- Is there any data on creating upsets in any of the devices listed above based on LET or other data that can help with their evaluation?
Regards,
-Mike