Hello!
I've encountered two differences between the design tool an the datasheet:
- The datasheet mentions 470 pF for C_VREF (Section 8.3.7), the picture in the design tool states 470 nF.
- Using an V_UVLO_ON of 8 V, an V_UVLO_OFF of 6 V and a R_UVT of 180 kOhm, I get an R_UVB of ~28,7 kOhm using the design tool. Using the same values in formula (3) in section 8.3.5 of the datasheet, I get 39,3 kOhm.
Can you tell me which information is correct in each case?
Best regards
Felix